Issue:
What is part 31161-184-52, and how can it be replaced?
Product Line:
NEMA Starter - GIC Product
Environment:
US Product
Cause:
Product Specification
Resolution:
The part number is found on the solid state overload relay used on a Class 8536 Type SG (Size 5) Series B starter. This part number identifies the solid state overload relay only. It does not include the wiring harness which is also required for this overload. 31161-184-52 is a restricted part number and cannot be ordered separately. The replacement options would be for the overload only (9065ST520) or for the overload, wiring harness, and current transformer block (9065SF520).
What is part 31161-184-52, and how can it be replaced?
Product Line:
NEMA Starter - GIC Product
Environment:
US Product
Cause:
Product Specification
Resolution:
The part number is found on the solid state overload relay used on a Class 8536 Type SG (Size 5) Series B starter. This part number identifies the solid state overload relay only. It does not include the wiring harness which is also required for this overload. 31161-184-52 is a restricted part number and cannot be ordered separately. The replacement options would be for the overload only (9065ST520) or for the overload, wiring harness, and current transformer block (9065SF520).
Released for:Schneider Electric USA