Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: How does the PKSB3 service barrier install into the QO, 3 phase, series S0__, (125 - 225 A) main circuit breaker load centers?
Issue:
Product Design Features

Product Line:
QO 3-Phase Load Centers

Resolution:
The PKSB3 service barrier is used ONLY with the QO, 3 phase, series S0__, (125-225A) main circuit breaker load centers.
The kit will contain 1 service barrier
The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.
A PDF copy of the complete instructions is attached below the video.

Danger label

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) After the service entrance wires(or conductors) have been properly installed, press the service entrance barrrier onto the service wires(or conductors), simultaneously, and into the mounting holes in the circuit breaker, until the barrier is fully seated. SEE FIGURE 1 of the instructions.
NOTE: The service barriers do not allow the load center to be serviced while energized. ALWAYS turn OFF all power to the load center before working on the load center.

NOTE: PLEASE MAKE SURE TO FOLLOW ALL THE INSTRUCTIONS THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric USA

Attachment(s)
PKSB3 Service Barrier.pdf [282.31 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings