How can we help you today?

What are the repair parts for the SC42M200PS, Series M01?

Issue:
Current Design Repair Parts

Product Line:
Combination Service Entrance Devices

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4056171950
Meter Cover Mounting Screw - 4020513002K (contains 10 screws; only two screws are required to secure the cover)
Utility Pullbox Cover - 4056194650 (includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover Assembly - 4056194350 (includes includes latch and hinges)
Load Center Cover Mounting Screws - 2142217101 (2 required)
Dead Front Interior Trim - EAV84023
Dead Front Interior Trim Mounting Screw - 4020513002K (contains 10 screws; only two screws are required to secure the interior trim)
Load Center Interior - MTR10004 (main breaker not included)
Load Center Interior Mounting Screw - 4020510001 (2 required)
Main Breaker - QOM2200VH (includes mounting screw 4020511201)
Main Breaker mounting keps nut - 2342702001 (2 required)
Meter Base - 7329882750 (phenolic base only; line and load meter jaws not included)
Meter Base Mounting Screw - 2142717200 (2 required)
Meter Socket Jaw - 7329794850 (4 required for complete meter socket, does include blade guide)
Meter Jaw Mounting Keps Nut - 2342702001 (1 per meter jaw)
Meter Jaw Blade Guide - 4052761901 (1 per meter jaw)
Meter Jaw with Blade Guide included - 7329746450 (4 required for complete meter socket and includes blue blade guide)
Meter Sealing Ring - 2920910001
Main Line Side Phase Lugs - 4025116051 (1 per phase)
Keps Nut for Main Line Side Phase Lugs - 2342702001 (1 per lug)

Load Center Cover Hasp and rivets - 4056174201 (hasp) and 2430393170 (rivets; 2 required)
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings