Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How to resolve error code 9.31 on the IG6 Line Isolation Monitor
Issue:
How to clear the ER9.31 error code on the LIM IG6?

Product Line:
LIM or Line isolation Monitor

Environment:
IG6M

Cause:
N/A

Resolution:
The 9.31 Error code indicates there is an internal program memory error. This will require replacing the LIM. The part number is IG6M. work with your local distributor to return the item and obtain a new one.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings