Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the new actuator AG13A020 be used on classic Erie Zone Valve Assembly?
Issue:
Can the new Erie PopTop actuator be used on a classic Erie Zone valve Assembly?

Product Line:
HVAC / Field Devices

Environment:
Valves and Actuator

Cause:
Replacement / Installation / Maintenance

Resolution:
No, the new PopTop actuators can't be used on the older Erie Classic Zone valve assemblies.
There are no available adaptors can be used for new actuators to fit on old assemblies. A new Zonw valve with actuator is needed for replacement of old Erie valve assembly.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings