What is the wire range for the main breaker and neutral used in a, EZM31000CB, series M02?
Issue:
Product design features
Product Line:
EZM metering
Resolution:
The Series M02 uses the PGP36100U31A main circuit breaker. The line lugs accept (4) 3/0 AWG - 500 kcmil Al/Cu conductors per phase and neutral.
Product design features
Product Line:
EZM metering
Resolution:
The Series M02 uses the PGP36100U31A main circuit breaker. The line lugs accept (4) 3/0 AWG - 500 kcmil Al/Cu conductors per phase and neutral.
Released for: Schneider Electric USA


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.