Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How is a DRK1020 class R fuse kit installed into the correct general duty safety switch fuse clips?
Issue:
Product design features

Product Line:
General Duty Safety Switches

Resolution:
The DRK1020 is a rejection pin inserted into a hole in the LINE SIDE fuse clips of a 100 ampere switch, or in the LOAD SIDE fuse clips of a 200 ampere switch. Pliers may be required to insert the rejection pins into the fuse clips. An insertion tab is included with the kit to aid in positioning the rejection pin. Remove the insertion tab once the rejection pin is inserted into the fuse clips. The rejection pins should not be able to be removed once properly installed. Three rejection pins are included with each kit.

Schneider Electric USA

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings