Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H321N, series F1 or F5? (may be shown as F01 or F05)
Issue:
Field replaceable parts for the H321N series F1 or F5 (may be shown as F01 or F05)

Product Line:
Safety Switch

Resolution:
The repair parts for the H321N, series F1 (F01) are as follows. No other parts are available.
Line Base Assembly -4056642450 (1 required; arc suppressor assembly not included)
Load Base Assembly - 4056641150 (1 required)
Arc Suppressor Assembly - 4056001801 (1 required)
Lug Assembly - 4025101652 (per lug)
Switch Mechanism - 4056610750
Handle Assembly - 4056684150K
Lockplate - 4056637601
Neutral Assembly - SN03
Neutral Bonding Screw - 4028365650

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings