How can we help you today?

What are the repair parts for the H321A, series F1? (may be shown as F01)

Issue:
What are the repair parts for the H321A, series F1? (may be shown as F01)

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the H321A, series F1 (F01) are as follows. No other parts are available.
Line Base Assembly -4056642850 (1 required; arc suppressor assembly not included)
Load Base Assembly - 4056641250 (1 required)
Arc Suppressor Assembly - 4056001801 (1 required)
Lug Assembly - CL0306F (includes 6 lugs)
Switch Mechanism - 4056610750
Handle Assembly - 4056684150K
Handle Gasket - 4056603101
Lockplate - 4056637601
Line & Load base mounting screw - 4020516001 (3 for line & 2 for load)
Arc Suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings