How can we help you today?

What are the repair parts for the HU363AWA, series F5 (may be shown as F05)?

Product Line:
Safety Switches

Resolution:
The Appleton Receptacle Switch catalog number HU363AWA has been Obsoleted and is no longer available consider using a different receptacle type switch.

The repair parts for the HU363AWA, series F5 (F05) are as follows. No other parts are available.
-Line Base Assembly - 4056614150 (1 required; arc suppressor assembly not included) (obsolete; replaced with 4056775250)
-Line Base Mounting Screw - 4020515101 (3 required)
-Arc Suppressor Assembly - 4056635550 (1 required) (obsolete; replaced with part number NNZ51874)
-Arc Suppressor Mounting Screw - 4020514501
-Handle/Mechanism kit - HMR10FN12 (includes handle, mechanism, rod, and lockplate)
-Lug Kit - CL10F (includes all line and load lugs)
-Receptacle - WRDK1034 (obsolete without replacement)
-Receptacle Mounting Screws - 4510280101 (4 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings