What is the operating temperature range of the 9007 type C lever limit switch?
Lever arm types: -28.9 degree C (-20 F) to 85 degree C (+185 F)
Plunger Arm Type and wobble stick Type 0 degrees F to 185 degrees F.
CTA-ID : 15719
Plunger Arm Type and wobble stick Type 0 degrees F to 185 degrees F.
CTA-ID : 15719