Can the HOM240GFI or HOM250GFI breaker be installed in the HOM24L70S load center?
Issue:
product design features
Product Line:
Homeline load centers
Resolution:
Yes, they can. However, when using an HOM-GFI breaker, the maximum wire size is #10 AWG.
product design features
Product Line:
Homeline load centers
Resolution:
Yes, they can. However, when using an HOM-GFI breaker, the maximum wire size is #10 AWG.
Released for: Schneider Electric USA










Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.