Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
I need the replacement powerplant for a NEMA size 2 Type S starter.
Issue:
PowerPlant part number for NEMA Size 2 Starter

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Contactors and Starters

Resolution:
The powerplant part number is 31063-016-54, and will not include the armature, magnet, or coil. (Obsolete already)
See instruction sheet for available parts

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings