What is the recommended torque for the joint bolt used on I-Line busway once the outer head Torque head of the Visi-Tite bolt has been twisted off?
Issue:
What is the required torque value for the joint bolt of an I-line busway?
Product Line:
I Line II Busway
Environment:
Installation
Resolution:
The recommended torque for the joint bolts of the I-Line II Busway is 70 lb-ft +/-10 lb-ft. The torque on the bolt should only be checked with the busway de-energized.
What is the required torque value for the joint bolt of an I-line busway?
Product Line:
I Line II Busway
Environment:
Installation
Resolution:
The recommended torque for the joint bolts of the I-Line II Busway is 70 lb-ft +/-10 lb-ft. The torque on the bolt should only be checked with the busway de-energized.
Released for: Schneider Electric USA
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.