How can we help you today?

How much force does it take to switch the handle of a KD, KG, or KJ circuit breaker?

Product Line:
Molded Case Circuit Breaker
Resolution:
Below are the required forces for the handle of the legacy K-Frame breaker.

OFF to ON =  5.5 lbs of force
ON to OFF = 8 lbs of force
TRIP to OFF = 11.5 lbs of force

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings