Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
HEPD50 to a breaker

Title: Can an HEPD50 or HEPD80 be connected to an existing breaker in the panel?

Issue: Can HEPD50 be connected to an existing 20 A breaker in the load center?

Product Line: Surge Protective Device

Resolution: It can be connected to an existing breaker as long as the breaker is rated to accept parallel wires per pole.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings