The enclosure
L600AWK will become suitable for service entrance equipment only when a
neutral assembly is installed. Please see available neutral assemblies for this enclosure below:
SN400LA (250 to 400 A rating)
SN1000MA (400 to 600 A rating)
Released for: Schneider Electric USA