Issue:
Require part number for Weathershield, Wall Mounting Bracket and Ceiling Mounting Bracket for 150 KVA 22M Enclosure Type EXN transformers.
Product Line:
LVGP Transformers
Environment:
Transformer Accessories
Resolution:
Part Numbers for the Weathershield is 7400WS22M and Ceiling Mounting Bracket is 7400CMB22M.
NOTE: Wall mounting bracket is unavailable for 22M enclosure type EXN transformers. Wall mounting brackets are used with units weighing no more than 700 lbs.
Released for: Schneider Electric USA