Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the maximum string size for the inverter MPPT strings?
The maximum string voltage must not exceed 600VDC. The voltage of a solar array increases as ambient temperature decreases so care must be taken to account for this voltage rise and the string sized to accommodate the LOWEST expected temperate of the site. The maximum short circuit rating of the modules on an MPPT channels must not exceed 16 amps.  We recommend that you refer to the Schneider Inverter data sheet and take our Solar Design Certification training to help determine the appropriate string length.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings