The number of loads that can be controlled will vary depending on the number of breakers in the panel and if used for partial or whole home backup. For partial home backup, you will only be able to control the loads on the essential/critical loads side.
In general, 120V relays use two spaces for two points of control. 240V relays use two spaces for one point of control up to 30 amps. 240V relays up to 60A uses four spaces for one point of control.
In general, 120V relays use two spaces for two points of control. 240V relays use two spaces for one point of control up to 30 amps. 240V relays up to 60A uses four spaces for one point of control.
Released for: Schneider Electric USA