PCS functionality would be a firmware upgrade, however PCS settings need to be configured at the time of commissioning. To use the features, the system would need to be re-commissioned when the firmware is released.
Released for: Schneider Electric USA