Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Will HCW and HCW-M accept Powerpact P frame breakers?

Issue:

Will a PJA36080U33A fit in HCW I-line panel?

Product Line:

I-line Panelboards

Answer:

HCW can accept up to L frame breaker only 600A maximum and for HCWM, it can accept M frame breaker 800A maximum. Both won't accept P frame breaker so PJA36080U33A won't work. For 800A, you can check on MJA36800E10.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings