Product Line:
Circuit Breakers
Environment:
Applies to PowerPact M, P and R
Resolution:
We have an offering for the Kirk Key Interlock using the JE suffix. This is available if the breaker isn't existing yet.
Once they order the 2000A breaker make sure to request for the JE suffix for the Kirk Key Interlock and padlock attachment.
The FAQ [link here ] for adding Kirk Key Interlock in an existing breaker is limited to JA and JK suffix only so the option for padlock is not included in there.
Released for: Schneider Electric USA