Issue:
What is the part number for the cover for Masterpact NW trip units?
Product Line:
MasterpacT NW
Resolution:
There are two different types depending on the installed trip unit.
For ammeter trip units, it is S33592, which is a clear plastic cover.
For power and harmonic trip units, it is S47067, which is an opaque gray cover: