Issue:
What does the -PL suffix mean for legacy PX/PE circuit breakers?
Product Line:
PX/PE Molded Case Circuit Breakers
Resolution:
PX/PE circuit breakers have a built-in (factory installed) padlocking feature for locking OFF only. An additional hinge over hasp feature is available on PX/PE to meet EUSERC requirements—add PL suffix.