How can we help you today?

Are Hermetically Sealed Contacts Compatible to 9001K/SK Joysticks?

Issue:

Need to find out if the Hermetically Sealed Reed contact blocks work on a 9001K/SK Joystick

Product Line:

30mm Joysticks

Environment:

Push Buttons and Operators

Resolution:

Yes, the hermetically sealed contacts 9001KA4* and 9001KA5* are compatible but there are limitations. The reed contacts can only be mounted on 1 side (either side), maximum of 2 in tandem.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings