Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Zelio : What are the programming languages that I can use for configuring Zelio Smart Relays?

Product Line:
Zelio Smart Relays

Environment:
Rail Mounted Programmable smart Relays

Cause:
Is it possible to change programming language from Function Block to Ladder Diagram and vice-versa?

Resolution:

There exists 2 different Programming languages, once a relay has already been setup on the smart relay controller it will adapt the topology of either ladder or function block layout for the respective I/O capabilities based on the commercial reference being used.

Ladder Language

A program that written in Ladder Languages is made up up of a series of ladder networks executed by the smart relay , a ladder network is build of graphic elements set out over a wiring sheets.

Ladder Mode Zelio Soft

Function Block Language

FBD mode allows graphic programming based on the use of predefined function blocks, to setup a function block program, the different functions need to be inserted in the wiring sheet this will allow us to Simulate and Monitor the program.

Function Block Mode Zelio Soft

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings