Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What can cause an INF31 or INFV fault on the ATV680 or ATV980 Drives?

Issue:

INF31 or INFV error on the ATV680 ATV980 Drive.


Product Line:

ATV680, ATV980, APM low harmonics


Environment:

All


Cause:

The topology of the device is not correct compared to the device type, one or multiple AFE or Braking Unit Options are not to recognized by the system.


Resolution:

- check the Modulink connection cables between the module link board (master control block) the AFE bricks and the braking unit option.

- check the termination resistors of the Modulink (120ohm resistance)

- check the Can Bus addresses of the AFE Bricks (starting at 20 on the right side)

- check the Can Bus addresses of the Braking unit option (starting at 40)

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings