ATV320 Loss of follower setup
Issue:
How is Loss of Follower or 4-20mA loss set up in ATV320 drive?
Resolution:
Goto DRI- > CONF > FULL > FLT > LFL > LFL3
Set LFL3 to desired setting such as LFF (Fallback Speed).
Goto DRI- > CONF > FULL > FLT > LFF > LFF
Set LFF (Fallback Speed) parameter to desired speed such as 60 hz.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)