Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can Profinet card be used with ATS480?

Issue:

Can Profinet card, VW3A3647 be used with ATS40 Softstarter?


Resolution:

The VW3A3647 option module version V3.2.12 and higher is compliant with
ATS480 product range with firmware V1.2 or higher. When the device has a
firmware version that does not support VW3A3647 option module, a [Internal
Error 6] INF6 error (see [Internal Error 6] InF6 Error, page 96 of the ATS480 manual) is triggered and a
firmware update of the device is required via SoMove.
NOTE: It is recommended to update device firmware without the option
module plugged in, otherwise a [Incorrect Config] CFF would be triggered
after the update.
The associated GSDML is named as the following example:
GSDML-V2.44-Schneider-ATS4X0-YYYYMMDD.xml
The files are available on www.se.com

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings