SAGE Config-to-Excel Tool Error When Loading Configuration Files
Issue
When attempting to open a configuration file in the SAGE Config to Excel tool for conversion, a warning message appears and the tool does not convert any data.
Product
SAGE Config to Excel Conversion Tool
Environment
Users converting SAGE configuration files—especially those generated by devices running Secure Firmware versions.
Cause
The tool was developed before the introduction of Secure Firmware.
Secure Firmware packages configuration files inside a compressed directory structure, and the tool cannot read the encrypted or zipped container directly.
Because of this, the tool fails to locate the XML data required for conversion and displays a warning.
Resolution
Before using the SAGE Config to Excel tool:
- Unzip the configuration file manually.
- Inside the extracted folder, locate the XML directory (usually named XML, ConfigXML, or similar).
- Point the tool directly to the XML folder instead of the compressed parent file.
Once the tool is directed to the XML contents, the conversion will work correctly.
Typical Error:
Suggested folder to point: