Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the difference between the ATS48 soft starter that has a part number that ends in Q versus one that ends in Y?

Article available in these languages: Tiếng Thái

Issue:
Difference between the ATS48 soft starter that has a part number that ends in Q versus one that ends in Y.

Product Line:
Altistart ATS48

Environment:
All serial numbers

Cause:
Customer in US is looking for an ATS48M10Q.

Resolution:
The ATS 48 ``Q`` was made for sale every where except the US.  It has 2 CT`s and a max voltage of 400 vac. The ``Y`` series has 3 ct`s and a max voltage of 690 vac.
If replacing an ATS48Q with a Y, it is very important to determine the full load amp rating of the motor. The ATS48**Q can be connected to the motor ``inside`` the Delta. This greatly reduces the amperage on each phase of the soft starter, allowing a smaller unit than normal to be applied to a motor. This is not currently possible with the ATS48**Y soft starters.
See the attached manual pages 92 to 94 (pages 11 to 13 of the electronic document)

Schneider Electric Việt Nam

Phần đính kèm
ATS48 Delta Motor wiring connections.pdf [23.71 KB]