The Temperature Thresholds at which the Cooling Fan of Altistart 48 Soft Starter start and stop is controlled are as follows:
1. Start – Heatsink Temperature > 50°C.
2. Stop – Heatsink Temperature < 40°C.
Đã phát hành cho: Schneider Electric Việt Nam