The main difference is that the SYBT5FR sku has batteries with flame retardant rated plastic. These are required in Japan. Unless the flame retardant specification is required the standard SYBT5 is recommended for use with Symmetra LX.
Đã phát hành cho:Schneider Electric Việt Nam