Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Why should cabinets be bonded to a common ground rather than use a cascading ground from cabinet to cabinet?
Issue:
Why does APC recommend that each cabinet be bonded to a common ground rather than cascade the ground from cabinet to cabinet?

Product Line:
NetShelter

Environment:
All versions and serial ranges.

Cause:
Questions may arise regarding bonding to a common ground vs. cascading.

Resolution:

By bonding each cabinet together in a cascading fashion the user relies on all of the cabinet frames in that ground path to reach the building ground.  If one cabinet is removed or one bad connection is made, the ground path is broken.  The easiest way to ensure a solid ground path is to run a common ground wire and connect each cabinet to it.

There may be a completely different viewpoint in regards to harmonics but that issue is at a very detailed engineering level, and is based on each individual location.
Our concern is that we recommend the most reliable physical method for bonding.