Hôm nay chúng tôi có thể giúp gì cho bạn?

Using PowerChute Network Shutdown in a redundant UPS Scenario

Issue:
The purpose of using Power Chute Network Shutdown with a redundant UPS configuration is to confirm that an event is occurring on all UPS before sending a shutdown signal to the connected servers.

Product Line:
Power Chute Network Shutdown

Environment:
All support OS

Cause:
Informational

Solution:

Information concerning configuring PCNS with redundant UPS can be found at this linkApplication Note #98