Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Uniflair Manual Start Up and Shut Down (PCO1)

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Uniflair Manual Start Up and Shut Down (PCO1)

Product line:
TDCVXXXX, TUCVXXXX

Environment:
All Serial Numbers

Cause:
Install/Repair

Resolution:

Start Up the Unit
1. Unlock the main switch.
2. Open the door and remove the closer panel if necessary.
3. Remove the metal screen from the electrical panel using a screwdriver.
4. Position all of the circuit breakers on the electrical board to “I” (on).

1

5. Install the cover metal sheet to the electrical panel and secure with the screws.
6. Verify all traps are pre-charged with water and all system pipes have been bled of air.
7. For internal pipe, it is necessary to remove the frontal security metal sheet.
8. Close the door and the front panels.
2
9. On the user interface, press the ENTER button. A sliding bar and a ventilator icon will appear on the display.  If an alarm is indicated, consult the Uniflair Chilled Water and Direct Expansion Operation and Maintenance manual.
Turn Off the Unit
1. On the first user interface screen, press the UP or DOWN buttons until the SWITCH OFF UNIT screen appears.
2. Press the ENTER button. The following icons will appear.
3. Press the ENTER button.
3

For additional information, see the Uniflair Chilled Water and Direct Expansion Operation and Maintenance manual.