Issue:
Command word for the ATS22 soft starters.
Product Line:
Altistart ATS22
Environment:
All
Cause:
Modbus address for ATS22
Resolution:
The command word address for the ATS22 soft starter is 752.
The ETA status word address for the ATS22 soft starter is 256
See the attached PDF document for the Command word and the ETA status bit assignments.
Đã phát hành cho: Schneider Electric Việt Nam