Issue:
Programming RY Relay for Run Status on ATV212 Drives.
Product line:
Altivar 212
Resolution:
Wire to RYA and RYC relay and program F130 to 14 (drive running). The relay will close if a run command is issued and there are no faults.
Đã phát hành cho: Schneider Electric Việt Nam