Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Altivar 61/71 what is the recommended corrective action when the motor runs in reverse with a run forward command?
Issue:
The motor is running backwards with a forward run command on the drive.

Product line:
Altivar ATV61 and ATV71

Environment:
All models, all serial numbers

Cause:
The phase rotation is inverted coming out of the drive going to the motor.

Resolution:

Option 1:
To correct the motor rotation swap two motor leads on the drive output terminals.

Option 2:
Go in the simple start menu 1.1 find output phase rotation change it from ABC to ACB.
Refer to the ATV61 and ATV71 programming manuals.