Issue:
ATS48 internal fan replacement selection
Product Line:
Altistart 48
Environment:
All models, all serial numbers
Cause:
Replacement and repair pars
Resolution:
The following list shows the softstart part number along with the part number and (quantity) of the fan kits needed for each softstarter.
ATS48D32Y - VZ3V481 (1)
ATS48D38Y - VZ3V481 (1)
ATS48D47Y - VZ3V4811 (1)
ATS48D62Y - VZ3V482 (1)
ATS48D75Y - VZ3V482 (1)
ATS48D88Y - VZ3V482 (1)
ATS48C11Y - VZ3V482 (1)
ATS48C14Y - VZ3V483 (1)
ATS48C17Y - VZ3V483 (1)
ATS48C21Y - VZ3V484 (1)
ATS48C25Y - VZ3V484 (1)
ATS48C32Y - VZ3V484 (1)
ATS48C41Y - VZ3V485 (1)
ATS48C48Y - VZ3V485 (1)
ATS48C59Y - VZ3V485 (1)
ATS48C66Y - VZ3V485 (1)
ATS48C79Y - VZ3V485 (2)
ATS48M10Y - VZ3V485 (2)
ATS48M12Y - VZ3V485 (2)
ATS48 internal fan replacement selection
Product Line:
Altistart 48
Environment:
All models, all serial numbers
Cause:
Replacement and repair pars
Resolution:
The following list shows the softstart part number along with the part number and (quantity) of the fan kits needed for each softstarter.
ATS48D32Y - VZ3V481 (1)
ATS48D38Y - VZ3V481 (1)
ATS48D47Y - VZ3V4811 (1)
ATS48D62Y - VZ3V482 (1)
ATS48D75Y - VZ3V482 (1)
ATS48D88Y - VZ3V482 (1)
ATS48C11Y - VZ3V482 (1)
ATS48C14Y - VZ3V483 (1)
ATS48C17Y - VZ3V483 (1)
ATS48C21Y - VZ3V484 (1)
ATS48C25Y - VZ3V484 (1)
ATS48C32Y - VZ3V484 (1)
ATS48C41Y - VZ3V485 (1)
ATS48C48Y - VZ3V485 (1)
ATS48C59Y - VZ3V485 (1)
ATS48C66Y - VZ3V485 (1)
ATS48C79Y - VZ3V485 (2)
ATS48M10Y - VZ3V485 (2)
ATS48M12Y - VZ3V485 (2)
Đã phát hành cho: Schneider Electric Việt Nam