Issue:
ATV61/ATV71 Dynamic Braking resistor connection
Product Line:
ATV61 ATV71
Environment:
All ATV61 and ATV71 drives
Cause:
Where do you connect the Dynamic Braking resistor?
Resolution:
It is suggested to connect the braking resistor between PA/+ and PB power terminal.
Consult the product Installation Manual for details.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Đã phát hành cho: Schneider Electric Việt Nam