Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Can equipment be installed on the floor of a NetShelter CX or CX Mini?
Issue:
A user may want to install equipment on the floor of a NetShelter CX or CX Mini.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Equipment doesn't all fit into the U-space provided.

Resolution:
Before installing any equipment on the floor of the NetShelter CX please check with the OEM manufacturer for their installation recommendations.
The floor of the NetShelter CX and CX Mini is solid. There is no airflow being introduced from directly below the floor.