Issue:
TJF fault on the ATV61/ATV71 drives
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
TJF means IGBT overheating caused by drive overheating
Resolution:
This fault appears when the estimated temperature of an IGBT is too high. It is a calculated measurement based on the switching frequency, drive output frequency, and motor current.
Check the size of the load, motor, and drive.
Reduce the switching frequency in menu 1.4
Wait for the motor to cool before trying to restart the drive.
Đã phát hành cho: Schneider Electric Việt Nam