Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
With VM Startup enabled, PowerChute Network Shutdown Fails to Restart a Fault Tolerant VM that it shut down.
Issue:
In addition to the Fault Tolerant VM failing to start, there are errors reported in the vSphere client for PowerChute Network Shutdown (PowerChute) attempting to start a secondary VM.

Product Line:
PowerChute Network Shutdown v3.1, 4.x, 5.x

Environment:
VMware

Cause:
This issue occurs if the vCenter Server goes offline during a shutdown sequence. PowerChute then fails to identify which VM is the primary and which is the secondary.

Resolution:
None. When the vCenter Server becomes accessible, PowerChute will be able to identify the primary VM and issue a startup command to it. The system will start the secondary VM.