Issue:
Unable to connect to SoMove Lite with ATV71.
Product Line:
Altivar 71
Environment:
All Models equal to and below firmware v1.5.5.0
Cause:
None
Resolution:
The compatibility table for SoMove supports the ATV71 at Firmware version level V1.5.5.0
Đã phát hành cho: Schneider Electric Việt Nam