Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How is the sleep/wake (low speed timeout) programmed on the ATV212 drives?

Issue:
Sleep/wake operation (low speed timeout)  programmed on the ATV212 drives.

Product Line:
Altivar ATV212

Environment:
All

Cause:
Allows the drive to shut off after running at a preset low speed for a preset period of time.

Resolution:
The sleep/wake threshold is defined as LL + F391.
The time period to trigger sleep mode is F256.
If the drive operates at or below the threshold (LL + F391) for a period of time (F256), the drive will decelerate to a stop and flash LStP.  It will remain stopped until the speed reference again exceeds the threshold (LL + F391).  The drive will then accelerate to the new reference.