Hôm nay chúng tôi có thể giúp gì cho bạn?

XBTL100 A second EQUIPMENT is available but button is NOT active in the Dailog table

Goals and Symptoms

Adding an EQUIPMENT table in the Configure Dialogue table screen. "Use Dialogue Table" is selected. A second EQUIPMENT is available. Is shown and selected in "EQUIPMENT available" list. But "Add table" button is NOT active

Facts and Changes

XBTL1000

Causes and Fixes

When you add an other EQUIPMENT , you can only use the alarm table function.
Now, the alarm table capacity is limited to 64 words. If this capacity is reach by the main EQUIPMENT, there is no more space to create an other one for a secondary EQUIPMENT. Then the "Add Table" button is not active.