Hôm nay chúng tôi có thể giúp gì cho bạn?

What Modbus function codes does the ETG100 support.

Issue
What Modbus function codes does the ETG100 support.

Product Line
TSXETG100

Environment
Windows 7

Resolution
The TSXETG100 gateway supports all Modbus function codes, unless IP Filtering has been enabled.

If IP filtering is enabled, the following read only function codes are supported.

1, 2, 3, 4, 7, 8, 11, 12, 17, 20, 24, 43, 100