No, we don't offer a filler module but we do offer a cover which can be placed over the backplane connector. Its part number is BMXXEM010 and there are 5 covers included in the package.
R-82117
Đã phát hành cho: Schneider Electric Việt Nam






Nhãn hiệu của chúng tôi
Chào mừng bạn đến với Trang web của Schneider Electric
No, we don't offer a filler module but we do offer a cover which can be placed over the backplane connector. Its part number is BMXXEM010 and there are 5 covers included in the package.
R-82117
Sản phẩm
Hỗ trợ
Công ty